Other Parts Discussed in Thread: STRIKE, LM3S8971, MOTORWARE, INA282, INA240
TM4C1294NCPDTi3
3 PWM pins routed into 3 GPIO ports triggering ADC samples produces unbroken robust sample data.
Tested 1k ohm between PWM/GPIO inputs reduced frequency of POR events. The PWM pins routed to GPIO are also shared by FET gate driver input. Suspect random spikes are flowing back into GPIO ports strike the ADC trigger. Spike does not seem to effect the PWM peripheral, only the ADC trigger initiator is inflicted. The 1k resistor adds considerable roll off PWM edges, adding higher R value may further distort edges and real time events.
Obviously the spike event is below GPIO ESD rail diodes ability to block. Wonder if a Schottky diode PWM output into GPIO input might stop reverse currents flow back to ground is a solution. Something bad is happening to cause POR of the MCU.
Why is the GPIO MUX pad not stopping voltage spikes from attacking the ADC trigger?
Forward post resolves FET (dv/dt) surges of PWM 100% duty cycle and dead band assertions. 08-06-2016
https://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/533844