Hi,
I'm trying to use the F021 Flash API (V02.01.01) forTMS570LS1227 in CCS V5.5.0.00077, but the following 17 errors were occurred while I tried to link the project:
error #16004-D: file "../TC50N_Driver/CPU_Internal/F021 Flash API/F021_API_CortexR4_BE_V3D16.lib<Async.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "../TC50N_Driver/CPU_Internal/F021 Flash API/F021_API_CortexR4_BE_V3D16.lib<Async.WithAddress.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "../TC50N_Driver/CPU_Internal/F021 Flash API/F021_API_CortexR4_BE_V3D16.lib<BlankCheck.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "../TC50N_Driver/CPU_Internal/F021 Flash API/F021_API_CortexR4_BE_V3D16.lib<FlashStateMachine.EnableEepromSectors.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
.........
I have upgraded the ARM complier tools to V5.1.14, but the problems still exist.
If I use CCS V6.1.1 the above problems are solved, but because some other reasons exist, I must use the CCS V5.5.0, what would cause this error, and where should I look to solve it ?
Thank you