Other Parts Discussed in Thread: HALCOGEN
Hello,
I am having trouble trying to step through the FreeRTOS example project provided for development with the RM57L843ZWTT. I work for a 3rd party programming company, so this development will eventually be used on our programming platform. I am using CCS Version: 6.1.2.00015 and generated the files from HALCoGen 04.05.01.
I have the device connected to the XDS100v2 debugger we have in house, and I can run the example_freeRTOSBlinky project without any issues by downloading the image to flash. The issue is we need to develop a project to erase/program/verify the flash so we need this to execute from RAM. I also cannot use the feature to swap the flash and ram because our software currently requires a higher RAM address and the motorola file I am generating needs to use the higher RAM location.
So, I manipulated the linker command file to move the relevant information to RAM address space, and I can build and connect to my target. At this point I am getting a 'No source available for "0xc750" ' or 'No source available for "0xC" ' error. If I ignore this and try to load my .out file I get the following failure:
CortexR5: Trouble Writing Memory Block at 0x8000000 on Page 0 of Length 0x7ff0: (Error -1065 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
CortexR5: File Loader: Verification failed: Target failed to write 0x08000000
CortexR5: GEL: File: C:\myWorkspace_RM57L_v1\freeRTOSBlinky\Debug\freeRTOSBlinky.out: Load failed.
My first goal is to just get the project running from RAM at the higher address range. I've attached my .cmd file and would appreciate some feedback on this development.
Regards,