Is the "MDL-BDC24" "Black Jaguar" able to run a Servodisc motor? i have 3 Kollmorgan U12M4 Servodisc Motors they run at 44v 9a with peak of 85a. i was wondering if 2 MDL-BDC24's in parallel can run one of these motors?
The reason why i would prefer a Jaguar is because they have proven themselfs to be reliable threwout my FIRST Robotics time. Also they have a built in Position control, Limit Switch, and they look like a good finished product.
The motors and controllers will be doing alot of work, because my project is a 3d Printer, so i am looking for acceracy down to less than a millimeter, i know the motors and table and encoders are capable of it because its orriginal perpose was an Axial Inserter from Universal Insturments. The table HAD a slew rate down to .02 mm. i would like to beable to come down close to that.