Part Number: TM4C129XNCZAD
Other Parts Discussed in Thread: UNIFLASH, TM4C1292NCPDT
Hi,
We have custom board with TM4C129XNCZAD microcontroller with super cap support.
S/W: TI-RTOS, TI-ARM Compiler 5.2.5
Whenever power fails, we save the context the board to Internal EEPROM. After this we intend to put the micro-controller in deep sleep so that super cap discharge reduced. We are using PK6 as GPIO pin for wakeup signal. We have 5 tasks running
The deep sleep initialization code is as below
//
// Enable Auto Clock Gating Control.
//
SysCtlPeripheralClockGating(true);
SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_GPIOK);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ADC1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_CAN0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_CAN1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_COMP0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_EMAC0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_EPHY0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_EPI0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOC);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOH);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOJ);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_HIBERNATE);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_CCM0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_EEPROM0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_FAN0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_FAN1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOL);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPION);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOP);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOQ);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOR);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOS);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOT);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C2);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C3);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C4);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C5);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C6);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C7);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C8);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_I2C9);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_LCD0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ONEWIRE0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_PWM0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_PWM1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_QEI0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_QEI1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_SSI1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_SSI2);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_SSI3);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER2);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER3);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER4);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER5);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER6);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER7);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART1);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART2);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART3);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART4);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART5);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART6);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART7);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UDMA);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_USB0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_WDOG0);
SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_WDOG1);
//
// Set the clocking for Deep-Sleep.
// Power down the PIOSC & MOSC to save power and run from the
// internal 30kHz osc.
//
SysCtlDeepSleepClockConfigSet(63, (SYSCTL_DSLP_OSC_INT30 |
SYSCTL_DSLP_PIOSC_PD | SYSCTL_DSLP_MOSC_PD));
//
// Set SRAM to Low power when in Sleep Mode.
//
//
SysCtlDeepSleepPowerSet(SYSCTL_LDO_SLEEP|SYSCTL_TEMP_LOW_POWER|SYSCTL_FLASH_LOW_POWER|SYSCTL_SRAM_LOW_POWER);
//
// Set LDO to 0.90V in Sleep.
//
//
SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);
We get an interrupt on power fail. The ISR posts an event. In the event after the context data has been saved.
The following code is called the microcontroller to sleep
//
// Go into Sleep Mode.
//
//SysCtlDeepSleep();
The current consumption measured across the micro-controller gets reduced from 120 mA to around 55 mA. The data sheet says it should well below 20 mA. Are all my initialization correct? Do I have to do anything to reduce the current consumption. Also I saw the micro-controller getting locked in. Both times I had to use uniflash to unlock the microcontroller.
TIA
Narendra