Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
Hi,
I am currently working on tm4c1294ncpdt. i have problem related to dumping or erasing the program from the controller. I have dumped one code on controller, later if i try to erase the code from controller its not erasing (cant even dump). I am using keil software and ulink2 debugger. I have tried with all clock levels for debugger. The code which i used first had logic related to UDP. Now the green LED of RJ45 connector is continuously blinking with higher speed. I am not able to access the controller now. Is there any way to erase the code which is on controller ? Please help me in identifying the problem and resolving it as soon as possible.