Part Number: TM4C1294NCPDT
Hi,
This is the problem related to TM4C1294NCPDT Ethernet communication with IPADDR_USE_STATIC mode.
I have connected TM4C1294NCPDT board in LAN and running enet_io example code.
I could able see IP address, subnet mask and default gate way in IPADDR_USE_DHCP mode.
IP address : 192.168.1.227
sunbnet mask : 255.255.255.0
IP address : 192.168.1.240
Also I could able to do communication with board in IPADDR_USE_DHCP mode.
lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP);
But If am using IPADDR_USE_STATIC mode, ui32NewIPAddress = lwIPLocalIPAddrGet();
function returns ip address 0. So I am not able to communicate.
I have written code for static mode as follows:
lwIPInit(g_ui32SysClock,pui8MACArray, 0xC0A80105, 0xFFFFFF00, 0xC0A801F0, IPADDR_USE_STATIC);
IP address : 192.168.1.05 (0xC0A80105)
sunbnet mask : 255.255.255.0 (0xFFFFFF00)
IP address : 192.168.1.240 (0xC0A801F0)
Can any one help on this problem?
Kiran