My working environment:
Code Composer Studio Version: 6.1.3.00034
TivaWare_C_Series-2.1.3.156
Board: EK-TM4C129XL Rev D
Windows 10 x64
Code sample: enet_io, path C:\ti\TivaWare_C_Series-2.1.3.156\examples\boards\ek-tm4c1294xl\enet_io
When I execute this code sample, I see the following information in debug UART output:
Waiting for IP.
Waiting for link.
Waiting for IP address.
IP Address: 169.254.104.26 // connects after 40 seconds, OK
To use static IP, I make the following change in the code:
// lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP);
lwIPInit(g_ui32SysClock, pui8MACArray, 0xC0A80A01, 0xFFFFFF00, 0, IPADDR_USE_STATIC); // // 192.168.10.1
PC network adapter is set to static IP 192.168.10.200, subnet mask 255.255.255.0
UART output:
Waiting for IP.
Waiting for link.
Waiting for IP address.
The board never connects. So, DHCP is working, and static IP doesn't work.
Code sample: enet_lwip doesn't work at all, both in DHCP and static IP.
For reference: old EK-LM3S9B92 board with enet_lwip code sample from Stellaris development kip works properly on the same computer, both with DHCP and static IP.