This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: TM4C1294NCPDTI MICROCONTROLLER SHORT BETWEEN 3.3V AND GND

Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: TM4C123GH6PM

Hi,

    I am facing problem with TM4C1294NCPDTI3 MICROCONTROLLER showing the ground and supply getting shorted.

The schematics is exactly same as tiva series launchpad.

Below are the steps followed

 1. Checked the bare PCB for any shorts.

2. Microcontroller and its related components are soldered.

3. No shorts are observed between uC pins.

4.Measured the resistance between +3.3v and Gnd it shows 330KOhms

5. Measured the resistance between VDDC and Gnd it shows 5.89KOhms

6. After Powering the Microcontroller the current drawn is 230mA and IC gets heated up. After Power OFF, The resistance between supply and GND is 1.5Ohms.

7. Replaced  with two new IC and the problem exists.

the IC part no is TM4C1294NCPDTI369AVC5W G4

Kindly Help..

7.