Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: SEGGER
Hello,
Is there any off board programmer for TM4C123GH6PM? I need to use it with CCS.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: SEGGER
Hello,
Is there any off board programmer for TM4C123GH6PM? I need to use it with CCS.
Thanks
Why do you need the chip programmed before soldering? I'm sure there is a more convenient engineering solution to your requirements...
Still, in that case, you will need a programming jig, a board with JTAG/SWD connections and one of QFP IC Sockets. Yamaichi is an example of a manufacturer.
The creation of such programming board is a complex project in itself - you'd like to add test GPIO's to ensure that the firmware is properly downloaded; you will also need a good and reliable additional bootloader solution, for your first firmware is surely going to be outdated even before you solder the IC into the definitive board. Finally, consider daisy chain programming, so that you can program more than one IC at a time. Your board could even be autonomous, with a controlling MCU that would automatically program any chip inserted into the socket - and that would probably be more convenient using the ROM bootloader and UART communication.
Regards
Bruno
CCS 7 supports the Segger J-Link, albeit there are some functions not supported in the CCS debugger. See Segger J-Link support appears to be incomplete in CCS 7.0.0.00022 and CCS/TM4C1290NCZAD: Cannot enable/disable (breakpoint) while the target is running when using J-link.Bruno Saraiva said:is that JLink compatible to CCS?
My experience of using a J-Link with CCS is using a Segger J-Link EDU (same hardware as the Segger J-Link base).Bruno Saraiva said:I assume I'm lazy to take my 5-year old yellow IAR JLink from the bottom of the drawer and try it myself
I don't know if the old yellow IAR J-Link is still supported, I found SEGGER Discontinues IAR Branded J-Links which says Segger discontinued the IAR Branded J-Links in 2011.
Inability to (even) respond to, "Why is their such need?" signals (strongly) that "such need" is NOT "well considered."
The "safety, flexibility & potential "re-programming" - offered ONLY by "ON-Board" programming - absolutely "overwhelms" any "off board" effort. It is good to see "helpers here" rejecting "poorly thought/considered" poster desires. When such posters, "Break so much - and so far - from the herd" (some) justification should be supplied. (and of course - there is NONE!)
Encouraging (very likely) poster missteps does not do them any favor!