Part Number: EK-TM4C1294XL
Tool/software: TI-RTOS
Hello,
I'm using the tcpecho example from TI RTOS for getting familiar with socket programming. The code is working fine.
I want to know whether it is possible to know in code whether ethernet cable has be connected or not.
From what I've seen, the code flow doesn't enter the while loop given below:
while ((clientfd =
accept(server, (struct sockaddr *)&clientAddr, &addrlen)) != -1) {
System_printf("tcpHandler: Creating thread clientfd = %d\n", clientfd);
/* Init the Error_Block */
Error_init(&eb);
/* Initialize the defaults and set the parameters. */
Task_Params_init(&taskParams);
taskParams.arg0 = (UArg)clientfd;
taskParams.stackSize = 1280;
taskHandle = Task_create((Task_FuncPtr)tcpWorker, &taskParams, &eb);
if (taskHandle == NULL) {
System_printf("Error: Failed to create new Task\n");
close(clientfd);
}
/* addrlen is a value-result param, must reset for next accept call */
addrlen = sizeof(clientAddr);
}
Is there any other way to know whether ethernet cable is connected or not in code??
Regards
Praveen