Part Number: EK-TM4C1294XL
Tool/software: TI C/C++ Compiler
Welcome to the Connected LaunchPad!!
Internet of Things Demo
Type 'help' for help.
"Current MAC: 001ab603243b
Obtaining IP...
Continuing in offline mode.
> IP Address Acquired: 192.168.43.185
Locating CIK... CIK found in EEPROM storage.
CIK: 598b68e622bf202f4ef78a7bd85c4b01954de72e
Connected! Type 'stats' to see data for this board.
> sta"
After this I can not type anything like stats in COM port window it is stop no update from Serial port I am edit program is like this...
1) In -qs_iot.c file
uint32_t g_ui32SW1Presses = 0;
uint32_t g_ui32SW2Presses = 0;
uint32_t g_ui32InternalTempF = 0;
uint32_t g_ui32InternalTempC = 0;
uint32_t g_ui32TimerIntCount = 0;
uint32_t g_ui32SecondsOnTime = 0;
uint32_t g_ui32LEDD1 = 0;
uint32_t g_ui32LEDD2 = 0;
uint32_t g_ui32LEDD3 = 0;
uint32_t g_ui32LEDD4 = 0;
uint32_t g_ui32LEDD5 = 0;
char g_pcLocation[50] = "";
char g_pcContactEmail[100] = "";
char g_pcAlert[140] = "";
tStat *g_psDeviceStatistics[NUM_STATS]=
{
&g_sSW1Presses,
&g_sSW2Presses,
&g_sInternalTempF,
&g_sInternalTempC,
&g_sSecondsOnTime,
&g_sLEDD1,
&g_sLEDD2,
&g_sLEDD3,
&g_sLEDD4,
&g_sLEDD5,
&g_sLocation,
&g_sBoardState,
&g_sContactEmail,
&g_sAlert,
NULL
};
void
UpdateLEDs(void)
{
//
// If either LED's global flag is set, turn that LED on. Otherwise, turn
// them off.
//
if(g_ui32LEDD1)
{
ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, GPIO_PIN_1);
}
else
{
ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
}
if(g_ui32LEDD2)
{
ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
}
else
{
ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
if(g_ui32LEDD3)
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_0, GPIO_PIN_0);
}
else
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_0, 0);
}
if(g_ui32LEDD4)
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_1, GPIO_PIN_1);
}
else
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_1, 0);
}
if(g_ui32LEDD5)
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_2, GPIO_PIN_2);
}
else
{
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_2, 0);
}
}
2) In qs_iot.h
#define NUM_STATS 16
3)In Pinout.c
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0 | GPIO_PIN_1);
MAP_GPIOPadConfigSet(GPIO_PORTN_BASE, GPIO_PIN_0 | GPIO_PIN_1,
GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2);
MAP_GPIOPadConfigSet(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2,
GPIO_STRENGTH_12MA, GPIO_PIN_TYPE_STD);
//
// Default the LEDs to OFF.
//
ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0 | GPIO_PIN_1, 0);
ROM_GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2, 0);
Please help me in this and what is the problem in this.......