This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
For a custom TM4C129XNCZAD board I have implemented a (flash based) ethernet bootloader.
Things work out fine for most of the time and I can program a new binary just fine. This process works out around 4 or 5 times in a row and then when trying again the "emac flash" bootloader is stuck and no new binary can be transferred. From debugging and looking at the server I think the bootloader is stuck in some very early stage and does not even send a BOOTP_Request.
I then need to power cycle the device and then bootloading works fine again.
some details:
when debugging in Code Composer I can see that the bootloader is stuck in bl_emac.c in a function called "PacketTransmit". in more detail, it is stuck in this while loop
while(g_psTxDescriptor[g_ui32TxDescIndex].ui32CtrlStatus & DES0_TX_CTRL_OWN) {}
The status on the server side (the side sending the magic packet) is that it never got a BOOTP_Request from the tiva since it tries to keep sending the magic packet.
Any help on how to debug / fix this issue would be great since power cycling is not an easy option.
Thanks,
Robert
Funny thing right after my comment had the very same thought but for reason custom PCB Ethernet differential pair layout is somewhat critical. Recommend for TM4c129x transformer TCT/RCT center tap decoupling caps 0.1uf or greater depending on plane or trace connection (1uf or greater), seemingly relative to +3v3 pull up noise level. SPMA056–October 2013
Robert Preissl said:I have the Tiva launchpad directly connected to my computer.
More specifically with a crossover cable as straight through cable will not work. Recall had grown the very same issue you report of TX descriptor OWN bit hang. Boot loader client was past working with a cross over cable and while(1) loop with a interrupt call ( (*((void (*)(void))(*(uint32_t *)0x2c)))(); After removing while loop test and directly invoking the function it stared to hang on the OWN bit for what ever reason.
It must be something to do with the velocity of execution timing after NVIC commands and invoking the BootP semaphore since it never hung when app punched into semaphore handler. The other thing is application loop is disabling NVIC interrupts just prior to entering INT 0x2c like below but without the while(1) loop Boolean switch being set when the OWM bit hangs in TXD.
// // Disable all processor interrupts. Instead of disabling them // one at a time (and possibly missing an interrupt if new sources // are added), a direct write to NVIC is done to disable all // peripheral interrupts. // HWREG(NVIC_DIS0) = 0xffffffff; HWREG(NVIC_DIS1) = 0xffffffff; // // Clear any active interrupts. If the boot loader uses // any interrupts, they will therefore respond as expected. // HWREG(NVIC_APINT) = (NVIC_APINT_VECTKEY | NVIC_APINT_VECT_CLR_ACT); // // Return control to the boot loader. This is a call to the SVC // handler in the boot loader. // (*((void (*)(void))(*(uint32_t *)0x2c)))(); //0x2c