This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Analog FAE asking what I suspect are dumb MCU questions, but I have a customer who is trying to design a small camera that would hook up to a CMOS image sensor (doesnt need to be very high resolution), snap a photo, encode that image data into some sort of easily storable data type, save it to flash (internal or external), and send that image through any available comm peripheral when asked by another system later in time.
Can any Tiva part do this? Do you guys know if there is another MCU or processor from TI that can? They had used a davinci in the past, but it was being under-utilized in this capacity, and now it is far too large for the small form factor camera module they are trying to design.
Thanks,
Brian
Thank you, this looks great. This especially:
The TM4C129x family of MCUs from Texas Instruments feature an integrated Ethernet PHY and MAC
with cryptographic modules and a large number of serial and parallel interfaces for control and sensor
data acquisition. Integrating a camera would require a dedicated camera interface or an external
programmable logic like field programmable gate array (FPGA) and complex programmable logic device
(CPLD) to interface a MCU to the camera. This design uses the EPI peripheral with a logic gate for
protocol conversion without needing an external FPGA or CPLD. Using EPI with the logic gate significantly
reduces the complexity of interfacing the camera to the TM4C129x device family while providing the
advantage of integrated PHY that allows network connectivity for a host of video monitoring applications.
Now, what I notice about this design is there are a few things that are unnecessary, like:
I need the absolute smallest version of this, and it sounds like the EPI is truly the only thing that matters for this application. follow up questions:
Thanks,
Brian
Thanks.
Can you address this question:
I think we will need to store the periodic still-image data in external flash. Is using the EPI to interface to the camera using up this peripheral such that I wont be able to communicate with external flash?