Part Number: TMS570LS1224
Hi,
we use the F021 Flash Library for the EEPROM emulation and it works fine with the IAR Workbench for ARM v8.11.1. With the latest version 8.11.3 there is a big problem. The library doesn't work anymore. The program still stucks at the busy flag and erase flag check after the flash erase command.
The warning (error) message of the IAR Workbench is as follows:
IAR ELF Linker V8.11.3.13950/W32 for ARM
Copyright 2007-2017 IAR Systems AB.
Warning[Lt009]: Inconsistent wchar_t size
FlashStateMachine.EnableEepromSectors.obj(F021_API_CortexR4_BE.lib) and 17 other objects have wchar_t size 16 bits
adc.o and 256 other objects have wchar_t size 32 bits
Warning[Li026]: the module "FlashStateMachine.EnableEepromSectors.obj(F021_API_CortexR4_BE.lib)" (and 17 other modules) do not contain information to support Virtual
Function Elimination
++ The following sections would have been initialized by copy but were
excluded because they were marked as possibly 'needed for init':
.text:Fapi_calculateFletcherChecksum (Utilities.CalculateFletcher.obj(F021_API_CortexR4_BE.lib) #11)
.text:Fapi_initializeFlashBanks (FlashStateMachine.InitializeFlashBanks.obj(F021_API_CortexR4_BE.lib) #12)
.text:Fapi_issueAsyncCommand (Async.obj(F021_API_CortexR4_BE.lib) #11)
.text:_Fapi_divideUnsignedLong (FlashStateMachine.InitializeFlashBanks.obj(F021_API_CortexR4_BE.lib) #11)
.text:_Fapi_issueFsmCommand (FlashStateMachine.IssueFsmCommand.obj(F021_API_CortexR4_BE.lib) #11)
.text:_scaleEEFclk (FlashStateMachine.ScaleFclk.obj(F021_API_CortexR4_BE.lib) #13)
.text:_scaleMainFclk (FlashStateMachine.ScaleFclk.obj(F021_API_CortexR4_BE.lib) #12)
It seems to be a problem with the wchar_t definition. IAR wchar_t is 4 bytes and the library uses 2 bytes for wchar_t.
Is there a library build with 4 bytes wchar_t available?
The only information from IAR about the change of the wchar_t is as follows:
- Changed size of wchar_t in version 8.10 and 8.11
Object files following the ARM ABI has a runtime attribute indicating the size of
wchar_t.In EWARM version 7.80 and earlier, the size of
wchar_twas 2 bytes wide and the runtime attribute was set accordingly.For EWARM version 8.10, the size of
wchar_twas 4 bytes wide but the value of the runtime attribute was not updated. Thus in 8.10 code is generated with 4 byte widewchar_tbut the object file is marked as ifwchar_tis 2 bytes wide.In EWARM version 8.11
Looking only at thewchar_tis 4 bytes wide and the runtime attribute is set accordingly.wchar_taspect this has the following implications:-
Combining object files built with 7.80 and 8.10 will not trigger any linker warning but if the application uses
wchar_t, the behavior will be unpredictable. -
Combining object files built with 8.10 and 8.11 will trigger a linker warning but the application should work even if it uses
wchar_t. -
Combining object files built with 7.80 and 8.11 will trigger a linker warning and if the application uses
wchar_t, the behavior will be unpredictable.
-
Could be found here: netstorage.iar.com/.../iccarm.ENU.html
Any ideas?
Kind regards,
Christian