Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Linux
Hello,
Is there an update on the ability to flash TIVA through Linux? In Windows environment we make sure the device comes up as a "Stellaris Device Firmware Upgrade" and then use the program dfuprog.exe through a command prompt to flash a dfu image. Is there anything equivalent that can be ran from Linux?
I found this earlier post though I don't see an official reply and the links in the original post are now inactive so I'm not sure if the page they reference has changed or is stil the same. e2e.ti.com/.../417569
Thanks,
Juan