Part Number: RM48L952
Hi,
I am creating a new thread here because there is no response to the below E2E for a week.
e2e.ti.com/.../2508776
Do we require to use MibSPI's CS line in Slave mode to read/write with different size and different group?
In our application RM48L952 is used as a SPI slave 3 pins only(without CS).
We would like to know what should be taken care of in order to
implement SPI read/write with different size of data in Slave mode?
I believe in case of master mode, we can read/write with different size if we
change the group, but in this case we are not able to start the communication
even if we change the group(except for group0).The CSHOLD bit is set to 1.
We are trying this on a LaunchPad.
Below E2E mentions that In MIBSPI Slave mode, the CS lines are used to specify which Transfer Group,
so is it mandatory to use CS line to read/write with different size and different group?
e2e.ti.com/.../1012758
PLease let me know do we need CS to implement this?
Best Regards
paddu