Part Number: TMS570LC4357
so there is an internal mapping from NHET1 to mibspi for the trigger. can I setup a NHET1[8] then as an edge capture and if there is a LOW on the NHET1[8] pin/pad it will somehow cause the MIBSPI to be triggered?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
so there is an internal mapping from NHET1 to mibspi for the trigger. can I setup a NHET1[8] then as an edge capture and if there is a LOW on the NHET1[8] pin/pad it will somehow cause the MIBSPI to be triggered?