Part Number: TM4C129ENCPDT
Hi Team,
I'd like to get some clarification on the capabilities of the TM4C129ENCPDT. We are looking to use this to decrypt a 2048-bit RSA payload but have couple key questions:
1) Can this even be done? The datasheet indicates the AES is noted to only support up to a 256-bit key. Not sure if this is the max spec or if the part has the ability to go further?
2) If 2048-bit decryption is supported, what is an achievable decryption time? Is 15ms achievable?
Thanks,
Mitchell