This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-TMS57004: Performing some task every one second using TMS57004

Part Number: LAUNCHXL-TMS57004
Other Parts Discussed in Thread: HALCOGEN

Dear All,

I need to perform some task in TMS57004 every one second?

How can I do that?

Is there any sample code available for it?

Regards,

Gunit

  • Gunit,

    The RTI (Real Time Interrupt) module can be configured to generate a periodic interrupt every second, or whichever time interval you desire. You can configure the RTI using HALCoGen. From the "Help" menu of HALCoGen, click on "Help Topics" and then open the "Examples" group (bottom-most). One of the examples is called "example_rtiBlinky.c". This will walk you through a complete example of configuring the RTI for the periodicity you need.