Part Number: TM4C123GH6PGE
Other Parts Discussed in Thread: LM3S1627
Hello everyone,
Thanks to everyone for suggesting in my previous posts.
I am working on a new project which is completely based on my previous project. In my previous application, we are using TM4C123GH6PGE microcontroller for controlling the 3-phase AC induction motor, in that we are using PWM technique and space vector modulation for converting input DC voltage to 3-phase AC. By using hardware we are sensing the 2-phase currents and applying to the motor inputs.In that we are using VFD (V/F) techniques for controlling the speed of the motor.
So now i want to replace the 3-phase induction motor to BLDC motor (requirement from client site). So i eagerly know that i can apply same hardware specification with TM4C123GH6PGE microcontroller.
If yes, what kind of changes required in software and hardware for operating and controlling speed of the BLDC motor.
If No, then what i have to do to solve this problem. I request you to please suggest me clearly about hardware and software changes if required.
Thanks,
Regards,
Srinu.V.