Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN,
Hi all,
I have tested the lwip example from" http://processors.wiki.ti.com/index.php/HALCoGen_Ethernet_Driver_and_lwIP_Integration_Demonstration" and also tried the loopback example code, both worked fine.
But, now when I am using the HALCoGen generated code for EMAC loopback example, receive is not happening. I have observed some changes in the HALCoGen generated code unlike the previous one.
Now I am using 'HALCoGen 04.07.00'. All the configurations done on HALCoGen is same as that of the previous one(Ethernet example code) .
Is there any new configurations to be done in this version of HALCoGen for proper working of Ethernet.
*NB: The controller is 'TMS570LC4357' , MII mode, FULL DUPLEX, 100Mbps speed, PHY - Marvell's 88Q1010.
kindly give solutions and advises ASAP.