Hello,
We are using the TMS570LC4357, we would like more information about the IOMM module.
In Table 6-3 and Figure 6-6 of Reference manual (spnu563a), the 'GIOB[2] Select' can be selected by by PINMMR[23..16].
Nevertheless, in the su-section 6.5.6 just above the Figure 6-6, it is written : "Therefore, the input from this terminal can optionally be connected to the
GIOB[2] input. This connection is enabled by setting PINMMR160[0]=0 and PINMMR160[1]=1"
Is it a mistake ? what is the byte of the PINMMR160 register to configure the GIOB[2] Select ?
Best regards,
Christopher