Part Number: TMS570LC4357
Hello,
please provide a support. I am currently facing to the DCAN FIFO issue described by the document "SPNZ232B–August 2015–Revised June 2018" and marked as DCAN#27. Correct order of CAN messages is absolutely critical for our application.
As I understood the described workaround: The RX FIFO can be still used, but IF2 should be just replaced by IF3 register. To make workaround more clear, is it necessary to use DMA for IF3 register set access? Is possible to configure DCAN to use RX FIFO and generate interrupt when IF3 is updated by message object from FIFO? I just want to avoid DMA usage. Please clarify this.
Thank you in advance.