This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: TMS570LC4357

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Hello,

I was trying to develop driver code and test app for TMS570LC4357 Ethernet driver and Marvell 88Q1010 PHY. I have tested the code in HDK board its working fine.

All tweaking need for Marvell 88Q1010 is done. 

The pins mappings  to Marvell 88Q1010 are the following.

MII_TX_CLK : U7

MII_TXEN : E4

MII_TXD[0] : U8

MII_TXD[1] : R1

MII_TXD[2] : T2

MII_TXD[3] : G4

MII_RXCLK : T4

MII_RX_DV : U6

MII_RXD[0] : U4

MII_RXD[1] : T3

MII_RXD[2] : U3

MII_RXD[0] : V3

The halcogen configuration with respect to the above pins is done, generated the code.

The PHY is outputting 25Mhz on its MII_TX_CLK pin.

It seems like the TMSxx is not detecting the TX_CLK signal, TX is not happening.

RX is working fine.

what all can be the reasons for this issue?

NB: unable to probe the MII_TX_CLK pin of TMSxx to check whether clk is being routed correctly, due to Complex board design.

Kindly give valuable suggestions.

warm regards

Anandhu Ramesh