Tool/software: Code Composer Studio
Hello,
I am writing a ros_embedded program using github.com/.../rosserial_tivac
I need to measure time, in order to make a loop execute a routine each 100ms.
Usually this is done with something like:
while(1) {
current_time = micros();
if(current_time - last_time >= 100000) {
// execute routine
}
}
In tiva-c there is the SysCtlClockGet() - which returns 80000000 - when the TM4C123 is running at 80Mhz.
Is there any way we can get the sysclock ticks? Basically, I would like to do a blink without delay in the TM4C.
Are there anyways to accomplish this other than the use of measuring the time / clock timers? (maybe the systick interrupt)
Either way, how do I measure time in the TM4C? Sometimes I just need to temporarily measure how long a routine takes for debugging purposes.
Best regards,
Can