Part Number: TMS570LS1114
Hello,
the first two questions are not answered. The TMS570LS1114 does not have a flash bank 1. Also I can not use it.
1) Is there any other double usage of the customer OTP memory?
2) Can we use the OTP ranges 0xF000_0010 - 0xF000_0FFF and 0xF000_E000 - 0xF000_E7FF without further restrictions?
3) Is there an overwrite possible? Can a second write access clear further bits of the OTP memory?
I think the answer is no. How is the protection implemented?
3a ) Is every byte protected against further writes?
3b ) Is the protection against further writes for each bank width (144 bit) or flash sector?