Part Number: TMS570LC4357
Hello,
I would like to test ECC Mechanism of L2RAMMW.
I have seen the Diagnostic test procedure described in Technical reference Manual to test 1 or 2 bit in error.
In this case RAMERRSTATUS[22,21,20,19,12,11,10, 4] are checked for the test.
With an other procedure, is it possible to test the following Bit in RAMERRSTATUS register :
Bit0 : CPUWE (CPU Write Single Error)
Bit1 : REME (Read ECC Malfunction Error. Indicates that the SECDED logic failed to correct a single bit error on the read of a read-modify-write operation)
Bit3 : WEME (Write ECC Malfunction Error. This bit Indicates that the SECDED logic failed to correct a single bit error
during a CPU write operation)
Bit5 : CPUWDE (CPU Write Double-bit Error. This bit indicates that an ECC uncorrectable (double bit) error was detected during write access)
Bit7 : RMWDE (Read-Modify-Write Double Bit Error. This bit indicates that an ECC uncorrectable (double bit) error was
detected during read access of the read modify write operation)
Best regards,
François