This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
WiFi Provisioning on EK-TM4C123GXL with rtos. Linker Error unresolved symbol sl_WlanProvisioning.
Trying out the Http echo example. need help.
Find attached build console output.
**** Clean-only build of configuration Debug for project tcpEchoCC3X00_EK_TM4C123GXL_TI ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 clean -O
cleaning ../src/sysbios ...
DEL /F "tcpEchoCC3X00_EK_TM4C123GXL_TI.hex" "configPkg\linker.cmd" "configPkg\compiler.opt" "tcpEchoCC3X00_EK_TM4C123GXL_TI.out"
DEL /F "EK_TM4C123GXL.obj" "sockets.obj" "tcpEchoCC3X00.obj"
DEL /F "EK_TM4C123GXL.d" "sockets.d" "tcpEchoCC3X00.d"
RMDIR /S/Q "configPkg\"
Could Not Find C:\Users\PVlab\workspace_v8\tcpEchoCC3X00_EK_TM4C123GXL_TI\Debug\tcpEchoCC3X00_EK_TM4C123GXL_TI.hex
Could Not Find C:\Users\PVlab\workspace_v8\tcpEchoCC3X00_EK_TM4C123GXL_TI\Debug\tcpEchoCC3X00_EK_TM4C123GXL_TI.out
Finished clean
**** Build Finished ****
**** Build of configuration Debug for project tcpEchoCC3X00_EK_TM4C123GXL_TI ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
Building file: "../tcpEchoCC3X00.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_32_00_06_core/xs" --xdcpath="C:/ti/tirtos_tivac_2_16_00_08/packages;C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages;C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages;C:/ti/tirtos_tivac_2_16_00_08/products/ndk_2_25_00_09/packages;C:/ti/tirtos_tivac_2_16_00_08/products/uia_2_00_05_50/packages;C:/ti/tirtos_tivac_2_16_00_08/products/ns_1_11_00_10/packages;C:/ti/simplelink_sdk_wifi_plugin_2_40_00_22/source;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -p ti.platforms.tiva:TM4C123GH6PM -r release -c "C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS" --compileOptions "-mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O4 --include_path=\"C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI\" --include_path=\"C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00\" --include_path=\"C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/oslib\" --include_path=\"C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include\" --include_path=\"C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI\" --include_path=\"C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b\" --include_path=\"C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/posix\" --include_path=\"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/include\" --define=ccs=\"ccs\" --define=PART_TM4C123GH6PM --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi " "../tcpEchoCC3X00.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring tcpEchoCC3X00.xem4f from package/cfg/tcpEchoCC3X00_pem4f.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
making C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI/src/sysbios/sysbios.aem4f ...
gmake[1]: Entering directory `C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI/src/sysbios'
clem4f C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/BIOS.c ...
asmem4f C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M ...
asmem4f C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch.sv7M ...
asmem4f C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm.sv7M ...
asmem4f C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/family/arm/m3/TaskSupport_asm.sv7M ...
arem4f BIOS.obj m3_Hwi_asm.obj m3_Hwi_asm_switch.obj m3_IntrinsicsSupport_asm.obj m3_TaskSupport_asm.obj ...
gmake[1]: Leaving directory `C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI/src/sysbios'
Build of libraries done.
clem4f package/cfg/tcpEchoCC3X00_pem4f.c ...
"package/cfg/tcpEchoCC3X00_pem4f.c", line 15655: warning #112-D: statement is unreachable
"package/cfg/tcpEchoCC3X00_pem4f.c", line 16141: warning #112-D: statement is unreachable
"package/cfg/tcpEchoCC3X00_pem4f.c", line 16376: warning #112-D: statement is unreachable
"package/cfg/tcpEchoCC3X00_pem4f.c", line 16596: warning #112-D: statement is unreachable
"package/cfg/tcpEchoCC3X00_pem4f.c", line 16795: warning #112-D: statement is unreachable
"package/cfg/tcpEchoCC3X00_pem4f.c", line 16976: warning #112-D: statement is unreachable
Finished building: "../tcpEchoCC3X00.cfg"
1 file(s) copied.
making ../src/sysbios/sysbios.aem4f ...
gmake[1]: Nothing to be done for 'all'.
Building file: "../EK_TM4C123GXL.c"
Invoking: ARM Compiler
"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O4 --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/include" --define=ccs="ccs" --define=PART_TM4C123GH6PM --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="EK_TM4C123GXL.d_raw" --cmd_file="configPkg/compiler.opt" "../EK_TM4C123GXL.c"
Finished building: "../EK_TM4C123GXL.c"
Building file: "../tcpEchoCC3X00.c"
Invoking: ARM Compiler
"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O4 --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/include" --define=ccs="ccs" --define=PART_TM4C123GH6PM --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="tcpEchoCC3X00.d_raw" --cmd_file="configPkg/compiler.opt" "../tcpEchoCC3X00.c"
Finished building: "../tcpEchoCC3X00.c"
Building file: "../sockets.c"
Invoking: ARM Compiler
"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O4 --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/Users/PVlab/workspace_v8/tcpEchoCC3X00_EK_TM4C123GXL_TI" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_00_08/products/bios_6_45_01_29/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/include" --define=ccs="ccs" --define=PART_TM4C123GH6PM --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="sockets.d_raw" --cmd_file="configPkg/compiler.opt" "../sockets.c"
Finished building: "../sockets.c"
making ../src/sysbios/sysbios.aem4f ...
gmake[2]: Nothing to be done for 'all'.
Building target: "tcpEchoCC3X00_EK_TM4C123GXL_TI.out"
Invoking: ARM Linker
"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O4 --define=ccs="ccs" --define=PART_TM4C123GH6PM --define=ccs --define=TIVAWARE -g --gcc --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi -z -m"tcpEchoCC3X00_EK_TM4C123GXL_TI.map" --heap_size=0 --stack_size=512 -i"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/lib" -i"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.4.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="tcpEchoCC3X00_EK_TM4C123GXL_TI_linkInfo.xml" --rom_model -o "tcpEchoCC3X00_EK_TM4C123GXL_TI.out" "./EK_TM4C123GXL.obj" "./sockets.obj" "./tcpEchoCC3X00.obj" "../EK_TM4C123GXL.cmd" -l"configPkg/linker.cmd" -l"C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b/grlib/ccs/Debug/grlib.lib" -l"C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b/usblib/ccs/Debug/usblib.lib" -l"C:/ti/tirtos_tivac_2_16_00_08/products/TivaWare_C_Series-2.1.1.71b/driverlib/ccs/Debug/driverlib.lib" -llibc.a
<Linking>
undefined first referenced
symbol in file
--------- ----------------
sl_WlanProvisioning <whole-program>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "tcpEchoCC3X00_EK_TM4C123GXL_TI.out" not built
>> Compilation failure
makefile:146: recipe for target 'tcpEchoCC3X00_EK_TM4C123GXL_TI.out' failed
gmake[1]: *** [tcpEchoCC3X00_EK_TM4C123GXL_TI.out] Error 1
makefile:142: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****ole output.
I imported from resource explorer. But here I am trying to port the sdk from cc3100 to cc3120.
Hence facing issues. Kindly help.
I have followed the steps in the cc3100 to cc3120 sdk migration guide.
Is it a hardware issue that TM4C devices are not supported or some kind of software compatibility issue?
Will there be no support for tm4c devices with cc3120 in the future?