Part Number: TM4C1231E6PM
Hi,
Could you please confirm that PF0 pin will be in NMI mode after reset(POR)?
The datasheet "5.1 Signal Description" mentions that two NMI pins will be in GPIO mode after reset.
"The NMI signal is the alternate function for two GPIO signals and functions as a GPIO after reset."
Meanwhile "10.4 Register Map" mentions it will be NMI.
"The default reset value for the GPIOCR register is 0x0000.00FF for all GPIO pins, with the exception
of the NMI and JTAG/SWD pins (see “Signal Tables” on page 1200 for pin numbers). To ensure that
the JTAG and NMI pins are not accidentally programmed as GPIO pins, these pins default to non-committable."
Please let us know which statement is correct.
If this pin will be NMI pin by default then do we need any external pull-up/down to avoid
any unnecessary NMI interrupts?
Best Regards
paddu