This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM problem when trying to unlock PF0 as input (I'm trying to use the button)

I'm using tiva launchpad. I succeed unlocking PF0 in a simple task to turn on and turn off led with SW0 (PF0). But when I attached that configure to my present project, it's not working. In my present project, I use PF4 to start the setting mode and update the setting(end setting mode). In setting mode, I use PF0 to increase the count and diplay the count to LCD. This is my code. Is there anything in my code affect to the PF0?

Thank you so much for your answers.

8360.main.c
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/systick.h"
#include "driverlib/adc.h"
#include "LCD.h"
#include "Delay.h"
#include "ADC.h"
#define ADCTaskPeriod 7000
#define SW4TaskPeriod 50
#define SW0TaskPeriod 10
int ADCTimeCount=0;
int ADCFlag=0;
int SW0TimeCount=0;
int SW0Flag=0;
int SW4TimeCount=0;
int SW4Flag=0;
int SW4Install=0;
uint8_t Temp;
uint8_t LimitTemp,Count;
//Hien thi nhiet do len LCD
void Temp_Update(void)
{
int a,b;
if (Temp<10)
{
SetCursor_LCD(2,10);
LCD_data('0');
LCD_data(Temp+0x30);
}
else
{
a=Temp/10;
b=Temp%10;
SetCursor_LCD(2,10);
LCD_data(a+0x30);
LCD_data(b+0x30);
}
}
//So sanh nhiet do do voi nhiet do cai dat
int TempCheck()
{
if(Temp > LimitTemp)
return 1;
else
return 0;
}
//Doc ADC, so sanh voi gia tri truoc, neu khac thi hien thi
void ADCTask(void)
{
static int saveTemp;
ADCProcessorTrigger(ADC0_BASE,3);
Delay_ms(500);
if (Temp != saveTemp)
{
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • Hi,
    Can you please elaborate your problem? I'm not clear with your description. What are you trying to do with PF0 and PF4?
  • Hi Charles,

    I've answered similar questions from this poster - perhaps I can assist here, too...

    Poster's code block follows:

    void SW0Task(void)
    {
    	if (!GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_0))
    	{
    		if (SW4Install == 1)    // test # 1
    		{
    			Count++;
    			int a,b;
    			if (Count<10)
    			{
    				SetCursor_LCD(1,10);
    				LCD_data('0');
    				LCD_data(Count+0x30);
    			}
    			else
    			{
    				a=Count/10;
    				b=Count%10;
    				SetCursor_LCD(1,10);
    				LCD_data(a+0x30);
    				LCD_data(b+0x30);
    			}
    		}
    	}
    }

    Does your code reach to the "test #1" point I've identified?     If so - your code has properly detected PF0.

    Are you (really) sure that pin PF0 connects to a switch on the LPad?     (I seem to recall that PF0 - due to its (nonsensical) NMI default - was avoided)    [good that!]

    Note too that the LPad's switch -  or your "user supplied switch" may bounce - which will cause your variable "Count" to increment (many) more times than you desire.     One simple cure is to delay w/in this function - so that the switch bounce interval has expired...

    Your first job is to determine if you reach the indicated test point upon switch activation...

  • Hi , hi Charles , first, sorry about my bad English made you confused and thank you for your help.
    , I can't reach to that test point upon switch activation, the SW4Install variable reach to 1 when I pressed the SW4 (I can see from the Expressions).
    I'm sure that PF0 connects to the right switch on the LPad. Like I said, it works with the simple task to turn On and Off led.
  • Greetings - if you "cannot reach Test Point #1" your issue may lie w/in hardware or software - or both.

    Have you a scope (ideally) or a DMM - with which to monitor PF0 - both w/the proper (mating) switch, "actuated & un-actuated?" The signal level into PF0 should "swing" between the full 3V3 voltage levels.

    Once that's been "test/verified" (kindly humor me - do this - even though you report (past) success) you must test to see if your "IF statement" (below) performs to your desire. Your IDE should enable you to monitor PF0 - which provides a "second - and independent confirmation" of PF0's being "pulled-up" (your code showed that) AND being responsive to "switch activation." (assumes that the LPad's switches "drive to ground."

    Note: should the LPad's switch - tied to PF0 - "drive INSTEAD to VCC (3V3) when active" - you must alter PF0 to include a "WPD" not the "WPU" shown in your code!     (WPD = weak pull-down resistor)

    if (!GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_0))

    Do keep in mind the tendency for most switches to "bounce" (i.e. "make & break contact" - sometimes lasting for several milliseconds.) You must "prevent" any "return" to that IF statement (now above) within the suspected "switch bounce interval." (via use of a delay)