Part Number: TMS570LS3137
Hi everyone,
My customer has a problem that Hercules aborts when running memcpy().
The value of the register at abort is as follows.
I do not know the cause, I want some advice.
Best regards,
Sasaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137
Hi everyone,
My customer has a problem that Hercules aborts when running memcpy().
The value of the register at abort is as follows.
I do not know the cause, I want some advice.
Best regards,
Sasaki
Hi Wang-san,
I confirmed with my customer.
QJ Wang said:
How did your customer use memcpy(): source address, destination address, and data length?
souce address : 0x001E0000
destination address : 0x0801D918
data length : 4byte
QJ Wang said:
If copying data to external RAM attached to EMIF, which type is the external memory configured as: normal, device or strongly-ordered?
BTW, the destination address should not point to flash memory.
Does the code make unaligned accesses to the flash?
memcpy() is transferring from internal FLASH to internal RAM.
QJ Wang said:
The CortexR4 CPU will sometimes get an abort when making an unaligned access near the physical end of the bank boundary.
Please refer to FMC#79, and FMC#80 in SPNZ195d.pdf
It did not correspond to the above errata.
Do you find any problems from the above?
Best regards,
Sasaki