Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva-c mcp2551 can transceiver do not work

Hello

im using an tiva-c launchpad to comunicate via CAN. I also use an mcp2551 can transceiver.

The thing is that i can not communicate because the rs and vref pins of the transceiver had the

voltage value = 2.5 V but the rs is connected with an 10K resitance to the ground and vref is not connected to anything.

Anyone knows how to solve this ?