Part Number: TMS570LS3137
Hi,
As a continuation of the thread :https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/765766
The question is regarding the errata "The errata spnz195G for "TMS570LS3137"
: "An offset error is introduced in the conversion result of any channel if a current is being injected into a shared input channel." , if the input voltage on a shared input ADC channel > VCCAD-0.3V and if there is an overlap for sampling windows of two ADCs."
1. The ADC configuration used is as below: ADC sampling frequency is 104.9869 KHz. ADC1 Group-1 and ADC2 Group-2 are not triggered simultaneously. ADC1 Group-1 gets triggered first and subsequently ADC2 Group-1 is triggered with approx.., 4 cycles delay. (ie. 4 * 1/160MHz = 0.025 uS).
In this case will there be an offset error?
2. The ADC inputs are driven with instrumentation amplifier AD8421, followed by RC filter (100ohm, 1nF). From the datasheet the maximum bias current is mentioned for IAOSB1=14uA and IAOSB@=12uA.
Can we calculate the maximum offset voltage at ADC1 in case of input at ADC2 > 4.7V as (14+12)uA x 100 =260uV ?
Thanks
Midhun.