Part Number: TMS570LC4357
Other Parts Discussed in Thread: TPS65381A-Q1, TPS65313-Q1
Hi,
I am looking for a programmable (or factory loading) PMICs to use with safety critical TI controller TMS570LC4357. So my question is, Can I use programmable (factory loaded) PMIC for safety critical (DAL A) design?
If yes, could you please suggest a PMIC (programmable or factory loaded) which has min 3/4 buck (5V to 3.3V, 1.4V, 1.2V), 3/4 LDOs (3.3V, 2.5V, 1.2V) and 1 boost (5V to 12V).
Input voltage range is 1 to 5V.
Thanks,
Kirana