Other Parts Discussed in Thread: HALCOGEN
Hello,
Within DCAN there are registers called
IF1CMD, IF2CMD Within those registers, there is a bit called BUSY. This above mentioned bit is set to 1 whenever CPU writes the MESSAGE NUMBER field of the above registers. Is that the one and only one condition due to which this BUSY bit will be set to 1 or there are more than one condition due to which this bit have the possibility to set to 1? Please help. Thank you. Regards Pashan