Part Number: TM4C1294NCPDT
I have an EK-TM4C129XL that is to be control from Matlab on PC over serial/UART.
The problem is that the transmissions from PC do not trigger the receive interrupt. I do not forget to "resume" before trying.
Please check if I correctly configure everything. Here is the relevant code.
void initPCInterface(uint32_t sys_clk)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, 0b00000011);
UARTConfigSetExpClk(UART0_BASE, sys_clk, 57600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
UARTFIFOEnable(UART0_BASE);
UARTFIFOLevelSet(UART0_BASE,UART_FIFO_TX2_8, UART_FIFO_RX2_8);
UARTIntEnable(UART0_BASE, UART_INT_RX);
UARTIntRegister(UART0_BASE, pcCommInterface);
IntPrioritySet(INT_UART0,0x20);//MEDIUM PRIORITY
IntEnable(INT_UART0);
}
void initGPIO(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB));
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, PB_MASK);
GPIOPinWrite(GPIO_PORTB_BASE, PB_MASK,0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOP));
GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, PP_MASK);
GPIOPinWrite(GPIO_PORTP_BASE, PP_MASK,0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE));
GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE, PE_MASK);
GPIOPinWrite(GPIO_PORTE_BASE, PE_MASK,0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOC));
GPIOPinTypeGPIOOutput(GPIO_PORTC_BASE, PC_MASK);
GPIOPinWrite(GPIO_PORTC_BASE, PC_MASK,0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOQ));
GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, PQ_MASK);
GPIOPinWrite(GPIO_PORTQ_BASE, PQ_MASK,0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOK));
GPIOPinTypeGPIOInput(GPIO_PORTK_BASE, PK_MASK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOD));
//Unlock PD7, default NMI
HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;
GPIOPinTypeGPIOInput(GPIO_PORTD_BASE, PD_MASK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOM));
GPIOPinTypeGPIOInput(GPIO_PORTM_BASE, PM_MASK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION));
GPIOPinTypeGPIOInput(GPIO_PORTN_BASE, PN_MASK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOA));
GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, PA_MASK);
}
int main(void)
{
{// limit scope of sys_clock
uint32_t sys_clock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
initGPIO();
initPCInterface(sys_clock);
}//sys_clock is popped from stack
IntMasterEnable();
while(true);
}
minimal Matlab test. Matlab successfully opens the port
clear
close all
s=serial('/dev/ttyS0',...
'BaudRate', 57600,'DataBits', 8,'Parity', 'none', ...
'StopBits',1, 'Timeout',2);
fopen(s);%successful
fprintf(s, 'rzzzzzklkll');%send something, does nothing
fclose(s);