Part Number: MSP-EXPCC430RFX
Dear TI engineer
I am using msp-expcc430RF development kit. However, it suddenly broke. When connecting to the power source 2V, the current is higher than 1 A. When using the meter to measure the Vin and GND pin, it shows that they are shorted. I guess it is because I accidently connect it to a charged capacitor (around 6v) while at the same time the Vin and GND is accidently connected by a naked wire( I use wire to extend the Vin and GND). As a result, some part of it is broken.
How to find and fix the broken part? Could you please provide the instruction in steps? Or, do you sell this satellite board alone?
It is urgent. Could you please also send this post to the e2e in China? Cause I am in hong kong, it's under Beijing time. Or should I post a same post in e2e china?
Here is the picture. The plastic port at the left is melted by hot air gun as I want to remove the capacitor at the Vin to check if it is broken. However, it is fine.