This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI Hercules Friends & Family,
Our customer would appreciate some input regarding F021 Flash usage.
They are having some difficulty getting the F021 library to work from RAM.
The HL_sys_link.cmd file seems to be configuring memory correctly;
In addition they tried setting RAM permissions to RWX (and MPU region in HALCoGen to allow execution); it did not help.
They also tried the compiler option --ramfunc and using the .TI.ramfunc align(32) to automatically copy the library during initialization; see commented out line in the USER CODE section.
When the code is running as soon as the following line is reached a prefetchEntry interrupt fires;
fapi_status = Fapi_initializeFlashBanks( SYS_CLK_FREQ );
I have included a screenshot from them below. Unless we are understanding the LR register wrong, it seems the fault originates at an address outside of the defined memory region (0x08080004)?
Another thing noticed is the RAM ECC region doesn’t seem to be initialized? This obviously doesn't seem normal.
Suggestions welcomed.
TY,
CY
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
/* USER CODE BEGIN (2) */
/* USER CODE END */
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x001FFFE0
FLASH1 (RX) : origin=0x00200000 length=0x00200000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0007eb00
/* USER CODE BEGIN (3) */
//RAMFUNC (RWX): origin=0x08070000 length=0x00010000
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
/* USER CODE BEGIN (5) */
/* USER CODE END */
.intvecs : {} > VECTORS
.text align(32) : {} > FLASH0 | FLASH1
.const align(32) : {} > FLASH0 | FLASH1
.cinit align(32) : {} > FLASH0 | FLASH1
.pinit align(32) : {} > FLASH0 | FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
FEE_TEXT_SECTION : {} > FLASH0 | FLASH1
FEE_CONST_SECTION : {} > FLASH0 | FLASH1
FEE_DATA_SECTION : {} > RAM
/* USER CODE BEGIN (6) */
.flashapi : load = FLASH0, run = RAM, LOAD_START(FlashApi_LoadStart), LOAD_END(FlashApi_LoadEnd), LOAD_SIZE(FlashApi_LoadSize), RUN_START(FlashApi_RunStart), RUN_END(FlashApi_RunEnd), RUN_SIZE(FlashApi_RunSize),
{
--library= "C:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE_L2FMC_V3D16.lib" (.text)
"C:\ti_workspace\iVM_Bootloader\Debug\source\Fapi_UserDefinedFunctions.obj" (.text)
}
// .TI.ramfunc align(32) : { "C:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE_L2FMC_V3D16.lib" (.text) } load=FLASH0, run=RAMFUNC, table(BINIT)
/* USER CODE END */
}
Hello David,
The CPSR register value was 0x397 (see screenshot).
The Flash functions were working fine until they apparently moved the library to RAM.
Any other words of wisdom you can share would be greatly appreciated!
TY,
Chris
Chris,
We have bootloader examples available here:
http://git.ti.com/hercules_examples/hercules_examples/trees/master/Bootloaders
The bootloader copies the F021 Flash API to RAM and execute APIs from RAM instead of Flash.
Please also take a look at below E2E thread which is relevant:
best regards,
David Zhou
David,
Thanks so much!
Interestingly, I don't see source available at the git link?
Can you comment?
TY,
Chris
Chris,
Source code is there.
and bl_flash.c is calling Flash API functions.
There is command file for each device, e.g.:
The file is bl_link.cmd.
best regards,
David Zhou
Chris,
I would like to point out the copy is done in the main function of bl_main,c:
void main(void)
{
g_pulUpdateSuccess[3] = 0x30002019; /*version number, 03.00, in 2019*/
uint32_t fnRetValue = 0;
/* Initialize SCI Routines to receive Command and transmit data */
sciInit();
/* Copy the flash APIs to SRAM*/
//_copyAPI2RAM_(&apiLoadStart, &apiRunStart, &apiLoadSize);
memcpy(&apiRunStart, &apiLoadStart, (uint32)&apiLoadSize);
Customer would need to do something similar for their application.
best regards,
David Zhou
Thank you David.
Appreciate the extra pointers and comments.
I think this will help a lot. Stay tuned.
Regards,
Chris
David,
I want to again thank you for your input. Quite helpful.
At this point in time, the code looks like a good reference for the customer; I believe their main issue at this point is related to permissions and/or ECC, etc.
No further actions at this point but I will update the thread if something short-term comes back. Otherwise, we will close it out.
TY,
Chris
David,
Again, thanks for your help. It appears the cache setting for the SRAM memory region might have been the main culprit.
At this point the customer's F021 routines are successfully executing from SRAM. They can read and erase/write to Flash memory with one caveat;
Now they're encountering an interrupt vector fault when attempting an erase of a sector in Flash Bank 0. Probably some sort of user configuration/setup issue. Again no further actions required on your end from this thread's perspective. I’ll keep you posted if otherwise.
Regards,
Chris
Chris,
Thanks for the update.
Just FYI: The interrupts are not disabled inside the flash APIs. It is recommended that customers disable the interrupts before calling flash API.
best regards,
David Zhou
Thanks again David,
Understood. The converse of that is that Users can have interrupts enabled during this Erase process as the API supports that. I am also asking where their code that performs the Flash operation is, specifically, since if the code is also located in Sector 0, that would be a problem as you can’t erase that area. Also, I'm asking where is the interrupt vector located (0x00-0x20?) and if they can try to Erase another Sector (such as 4) only to see if that shows different behavior.
TY,
Chris