Part Number: TMS570LS3137
Hi Team,
Could see from the case - "https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/251397?tisearch=e2e-sitesearch&keymatch=ESMLTCPR" below details are missing in the TRM (spnu499c.pdf).
"The ESMLTCPR bit 15:14 are the only bits that you can change. Bit 13:0 is default to all 1's and these are read only bits.If you look at the TRM, the bit 15:14 is denoted as R/W while bit 13:0 denoted as R-1. I agree that it is a little bit confusing, but it is actually all 1's."
The value to be configured is R-1 instead of R (VCLK cycles) is missing in specific. Can we have these details added in the document?