This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS570LC4357: TMS570LC43x SPNU563A - Parity Compare Logic in SCM

Part Number: TMS570LC4357


Tool/software: TI C/C++ Compiler

Hi,

I read this post https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/382385?tisearch=e2e-sitesearch&keymatch=scmcntrl 

I have a follow on question to this post.  The post says to clear parity error flags in DMA, L2FMC and L2RAMW.  When I set SCMCNTRL to 0x0A050505 to start the transaction parity test, I do not see any parity error being set in L2FMC.  I was expecting to see parity error being set on FEDAC_PASTATUS, FEDAC_PBSTATUS, L2FMCPOM_POMFLG registers, but they are all 0x0 in Code Composer. Is this expected?  

Also, for L2RAMW, I only see RAMERRSTATUS CPEOI bit being set.  Should I expect bit MSACP, PACE to be set too?

Thanks!

JC