Hi all,
As mentioned in the below link feedback,
e2e.ti.com/.../602843
In small PCB, We have connected the 2 microcontrollers CAN channel with shorter distance.
But, CAN communication is not working with lower baud rate.
Microcontroller1 Microcontroller2
CANTX => CANRX
CANRX <= CANTX
With this option, whether CAN communication will work (or) not ?
https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf
Below are the clarifications,
#As mentioned, in the above link proposed diagram, Do we need to short both the pins and use along with diode ?
#In case if we are using CAN bus with diode option, Is there any performance degrading will happen? Eg: More Traffic in the CAN bus
Kindly give your valuable feedback.
Thank you.
Regards,
S.Saravanakumar