Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: CC3100
I have loaded on EK-TM4c1294XL connected launchpad the enet_io example and it runs ok only if I use browsers within the subnet of my house, if i try to access the web page from a browser outside this home net (subnet), the web page does not load. the main modem which supplies the internet wifi signal to my house is ARRIS TG862, and I checked with my Internet provider (CLARO) if there was a modem configuration that could be blocking the connection, but they have tested and tried to acces the web page with the IP address that enet_io provides by means of the terminal, and they could not either acess it.
I have tried with TM4C1294 and CC3100 booster pack to obtain web based io, using ek-tm4c1294xl-boost-cc3100 uvision project and no connection or access to internet is obtained, only there is communication between my celular and the board (TM4C1294 +boost cc3100). Will these two behaviors be related?. Please Help.