Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: Ethernet Communication Between Launchpad and PC

Part Number: EK-TM4C1294XL

Hello,

I would like to implement a communication via Ethernet between EK-TM4C1294 and a PC. PC is going to be the server and I would like just to pass 8bit data through Ethernet between the two.

Is there any related example performing this task?

Thank you.

  • Hello Alex,

    Have you looked at the enet_io example from TivaWare? TivaWare download available at: http://www.ti.com/tool/SW-TM4C

    Also within the docs folder of TivaWare you can find the User Guide for the EK-TM4C1294XL which offers descriptions of each example provided with TivaWare.

    Lastly, there are a set of examples for TI-RTOS for Tiva-C which covers Ethernet, so you may want to check those as well: www.ti.com/.../TI-RTOS-MCU
  • I saw enet_io. This example is going to help me later in my project.
    Firstly I would like to establish just a LAN connection between PC and TM4C1294XL in order to pass data.
    I don't want to use any online server.
    I have already establish a connection via USB and I want to do the same via Ethernet.
    Thank you
  • We don't have any other examples in TivaWare other than what you have seen. You can use the enet_io or the enet_lwip example as a starting and replace the enet_lwip.c with the below code. This will create an echo server using UDP. If you want TCP echo examples you can refer to the below two links. There are TI-RTOS based tcp and udp echo examples if you want to use TI-RTOS and the tcp stack that is based on the TI's NDK. 

    //*****************************************************************************
    //
    // enet_lwip.c - Sample WebServer Application using lwIP.
    //
    // Copyright (c) 2013-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.1.4.178 of the EK-TM4C1294XL Firmware Package.
    //
    //*****************************************************************************
    
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "driverlib/flash.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/gpio.h"
    #include "driverlib/rom_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/systick.h"
    #include "utils/lwiplib.h"
    #include "utils/ustdlib.h"
    #include "utils/uartstdio.h"
    #include "drivers/pinout.h"
    #include "lwip/udp.h"
    
    
    
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Ethernet with lwIP (enet_lwip)</h1>
    //!
    //! This example application demonstrates the operation of the Tiva
    //! Ethernet controller using the lwIP TCP/IP Stack.  DHCP is used to obtain
    //! an Ethernet address.  If DHCP times out without obtaining an address,
    //! AutoIP will be used to obtain a link-local address.  The address that is
    //! selected will be shown on the UART.
    //!
    //! UART0, connected to the ICDI virtual COM port and running at 115,200,
    //! 8-N-1, is used to display messages from this application. Use the
    //! following command to re-build the any file system files that change.
    //!
    //!     ../../../../tools/bin/makefsfile -i fs -o enet_fsdata.h -r -h -q
    //!
    //! For additional details on lwIP, refer to the lwIP web page at:
    //! savannah.nongnu.org/.../
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Defines for setting up the system clock.
    //
    //*****************************************************************************
    #define SYSTICKHZ               100
    #define SYSTICKMS               (1000 / SYSTICKHZ)
    
    //*****************************************************************************
    //
    // Interrupt priority definitions.  The top 3 bits of these values are
    // significant with lower values indicating higher priority interrupts.
    //
    //*****************************************************************************
    #define SYSTICK_INT_PRIORITY    0x80
    #define ETHERNET_INT_PRIORITY   0xC0
    
    //*****************************************************************************
    //
    // The current IP address.
    //
    //*****************************************************************************
    uint32_t g_ui32IPAddress;
    
    //*****************************************************************************
    //
    // The system clock frequency.
    //
    //*****************************************************************************
    uint32_t g_ui32SysClock;
    
    //*****************************************************************************
    //
    // Volatile global flag to manage LED blinking, since it is used in interrupt
    // and main application.  The LED blinks at the rate of SYSTICKHZ.
    //
    //*****************************************************************************
    volatile bool g_bLED;
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    
    void udp_echo_init( void );
    
    //*****************************************************************************
    //
    // Display an lwIP type IP Address.
    //
    //*****************************************************************************
    void
    DisplayIPAddress(uint32_t ui32Addr)
    {
        char pcBuf[16];
    
        //
        // Convert the IP Address into a string.
        //
        usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff,
                (ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff);
    
        //
        // Display the string.
        //
        UARTprintf(pcBuf);
    }
    
    //*****************************************************************************
    //
    // Required by lwIP library to support any host-related timer functions.
    //
    //*****************************************************************************
    void
    lwIPHostTimerHandler(void)
    {
        uint32_t ui32NewIPAddress;
    
        //
        // Get the current IP address.
        //
        ui32NewIPAddress = lwIPLocalIPAddrGet();
    
        //
        // See if the IP address has changed.
        //
        if(ui32NewIPAddress != g_ui32IPAddress)
        {
            //
            // See if there is an IP address assigned.
            //
            if(ui32NewIPAddress == 0xffffffff)
            {
                //
                // Indicate that there is no link.
                //
                UARTprintf("Waiting for link.\n");
            }
            else if(ui32NewIPAddress == 0)
            {
                //
                // There is no IP address, so indicate that the DHCP process is
                // running.
                //
                UARTprintf("Waiting for IP address.\n");
            }
            else
            {
                //
                // Display the new IP address.
                //
                UARTprintf("IP Address: ");
                DisplayIPAddress(ui32NewIPAddress);
                UARTprintf("\nEcho Server is ready.\n");
            }
    
            //
            // Save the new IP address.
            //
            g_ui32IPAddress = ui32NewIPAddress;
        }
    
        //
        // If there is not an IP address.
        //
        if((ui32NewIPAddress == 0) || (ui32NewIPAddress == 0xffffffff))
        {
            //
            // Do nothing and keep waiting.
            //
        }
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for the SysTick interrupt.
    //
    //*****************************************************************************
    void
    SysTickIntHandler(void)
    {
        //
        // Call the lwIP timer handler.
        //
        lwIPTimer(SYSTICKMS);
    
        //
        // Tell the application to change the state of the LED (in other words
        // blink).
        //
        g_bLED = true;
    }
    
    //*****************************************************************************
    //
    // This example demonstrates the use of the Ethernet Controller.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t ui32User0, ui32User1;
        uint8_t pui8MACArray[8];
    
        //
        // Make sure the main oscillator is enabled because this is required by
        // the PHY.  The system must have a 25MHz crystal attached to the OSC
        // pins. The SYSCTL_MOSC_HIGHFREQ parameter is used when the crystal
        // frequency is 10MHz or higher.
        //
        SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ);
    
        //
        // Run from the PLL at 120 MHz.
        //
        g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                                 SYSCTL_OSC_MAIN |
                                                 SYSCTL_USE_PLL |
                                                 SYSCTL_CFG_VCO_480), 120000000);
    
    
        PinoutSet(true, false);
    
        //
        // Configure UART.
        //
        UARTStdioConfig(0, 115200, g_ui32SysClock);
    
        //
        // Clear the terminal and print banner.
        //
        UARTprintf("\033[2J\033[H");
        UARTprintf("Ethernet lwIP udp echo example\n\n");
    
        //
        // Configure Port N1 for as an output for the animation LED.
        //
        MAP_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_1);
    
        //
        // Initialize LED to OFF (0)
        //
        MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, ~GPIO_PIN_1);
    
        //
        // Configure SysTick for a periodic interrupt.
        //
        MAP_SysTickPeriodSet(g_ui32SysClock / SYSTICKHZ);
        MAP_SysTickEnable();
        MAP_SysTickIntEnable();
    
        //
        // Configure the hardware MAC address for Ethernet Controller filtering of
        // incoming packets.  The MAC address will be stored in the non-volatile
        // USER0 and USER1 registers.
        //
        MAP_FlashUserGet(&ui32User0, &ui32User1);
        if((ui32User0 == 0xffffffff) || (ui32User1 == 0xffffffff))
        {
            //
            // We should never get here.  This is an error if the MAC address has
            // not been programmed into the device.  Exit the program.
            // Let the user know there is no MAC address
            //
            UARTprintf("No MAC programmed!\n");
            while(1)
            {
            }
        }
    
        //
        // Tell the user what we are doing just now.
        //
        UARTprintf("Waiting for IP.\n");
    
        //
        // Convert the 24/24 split MAC address from NV ram into a 32/16 split MAC
        // address needed to program the hardware registers, then program the MAC
        // address into the Ethernet Controller registers.
        //
        pui8MACArray[0] = ((ui32User0 >>  0) & 0xff);
        pui8MACArray[1] = ((ui32User0 >>  8) & 0xff);
        pui8MACArray[2] = ((ui32User0 >> 16) & 0xff);
        pui8MACArray[3] = ((ui32User1 >>  0) & 0xff);
        pui8MACArray[4] = ((ui32User1 >>  8) & 0xff);
        pui8MACArray[5] = ((ui32User1 >> 16) & 0xff);
    
        //
        // Initialize the lwIP library, using DHCP.
        //
    
        lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP);
    
    
    
     
        udp_echo_init();
    
        //
        // Set the interrupt priorities.  We set the SysTick interrupt to a higher
        // priority than the Ethernet interrupt to ensure that the file system
        // tick is processed if SysTick occurs while the Ethernet handler is being
        // processed.  This is very likely since all the TCP/IP and HTTP work is
        // done in the context of the Ethernet interrupt.
        //
        MAP_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY);
        MAP_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);
    
        //
        // Loop forever, processing the LED blinking.  All the work is done in
        // interrupt handlers.
        //
        while(1)
        {
            //
            // Wait till the SysTick Interrupt indicates to change the state of the
            // LED.
            //
            while(g_bLED == false)
            {
            }
    
            //
            // Clear the flag.
            //
            g_bLED = false;
    
            //
            // Toggle the LED.
            //
            MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1,
                             (MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1) ^
                              GPIO_PIN_1));
        }
    
    
    
    
    }
    
    void udp_echo_recv(void *arg, struct udp_pcb *pcb, struct pbuf *p, struct
    ip_addr *addr, u16_t port)
    {
        if (p != NULL) {
            /* send received packet back to sender */
            udp_sendto(pcb, p, addr, port);
            /* free the pbuf */
            pbuf_free(p);
        }
    }
    
    
    void udp_echo_init(void)
    {
        struct udp_pcb * pcb;
    
        /* get new pcb */
        pcb = udp_new();
        if (pcb == NULL) {
            LWIP_DEBUGF(UDP_DEBUG, ("udp_new failed!\n"));
            return;
        }
    
        /* bind to any IP address on port 23 */
        if (udp_bind(pcb, IP_ADDR_ANY, 23) != ERR_OK) {
            LWIP_DEBUGF(UDP_DEBUG, ("udp_bind failed!\n"));
            return;
        }
    
        /* set udp_echo_recv() as callback function
           for received packets */
        udp_recv(pcb, udp_echo_recv, NULL);
    }
    

  • I manage to implement an Ethernet communication between pc and TM4C1294XL.
    I set up a server application in Python and manage to send and receive data to launchpad in which I assigned a static IP address.
    The problem now is that I have to reset launchpad every time I want to send/receive data, in order communication between server/client to be established.
    Is there any way to establish communication every time I plug the Ethernet cable?
    Thank you!
  • What were you running on the LaunchPad? Have you try to use DHCP address? Does it make a difference?