Tool/software: Code Composer Studio
I wrote a software code to communicate 2 EK-TM4C1294XL launchpad using Ethernet; I configured the Ethernet speed to 100Mbps and full duplex communication; when I measured the transmission speed I found it about 87Mbps for transmitting 1500 bytes of data, but the receiving speed is about 16Mbps up to 20Mbps and down to 10Mbps.
In Ethernet communication, Is this receiving speed normal?