Part Number: TMS570LS1224
Other Parts Discussed in Thread: TMS5701224
Hi,
This is related the code for RM46 to enter low power mode.
To use it on TMS5701224 MCU I changed the target configuration file (in Properties > General) to match my device and changed the debug probe to the one I'm using. Is there anything else I need to adapt this code for TMS5701224?
I'm not sure if I damaged the something by using the code like that since now even after POR I always get this error:
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.0.27.9)
Regards,
Leslie