Part Number: TMS570LS0914
Tool/software: Code Composer Studio
Hello,
I am using FLASH API F021 for program TMS570LS0914.
After the sectors erased, I wrote to Flash . The address strated from 0x00020000 in sector7,ban0. The first time,I wrote 4094bytes(not 4096bytes)and succeeded. But the second time,I failed writing the successive 4094bytes (The address strated from 0x00020FFE).
I wonder if there is a limit to the least number of bytes (length of data to wirte once)? Maybe 4 or 16 bytes?
TMS570LS0914 is 32-bit microprocessor.Did I made a mistake about this? Should I write to flash by at least 4 bytes(32 bits)?
I am so coufused why the first time I succeeded but the second time I failed on writing to flash by 4094bytes. Please help me. I`ll be very appreciate!