This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I've implemented a CAN bus bootloader according to SPNA241 on TMDS570LS31HDK and TMDX570LC43HDK. Example have been fully realized just on TMDS570LS31HDK. But on TMDX570LC43HDK I've got an issue with software reset after loading application into the flash. It looks like CPU hanging after the software reset.
To explore the issue a simple test was created. Led blinks three times before software reset.
int main(void) { /* USER CODE BEGIN (3) */ int i, j; //Configure as output hetREG1->DIR = (1 << 5); while(1) { //three blinks before reset for(j = 0; j < 6; j++) { gioToggleBit(hetPORT1, 5); for(i = 0; i<5000000; i++); } //software reset systemREG1->SYSECR = (0x10) << 14; }; /* USER CODE END */ return 0; }
On TMDS570LS31HDK the led blinks continuously, but on TMDX570LC43HDK just three times. New cycle of three-times blinking on TMDX570LC43HDK can be initialized just by POWERON_RESET.
First running of gioToggleBit() function after SW reset gives data abort exception. In particular, the last instruction in following code.
gioToggleBit(): 00002c40: E24DD008 sub r13, r13, #8 00002c44: E58D1004 str r1, [r13, #4] 00002c48: E58D0000 str r0, [r13] 381 if ((port->DIN & (uint32)((uint32)1U << bit)) != 0U) 00002c4c: E59D0000 ldr r0, [r13] 00002c50: E59DC004 ldr r12, [r13, #4] 00002c54: E3A01001 mov r1, #1 00002c58: E5900004 ldr r0, [r0, #4]
I used CCS Version: 10.0.0.00010, HALCoGen 04.07.01
Can you help to solve the issue with TMDX570LC43HDK?
Regards,
Sergey
Hello, Wang!
Thank you for quick reply!
As I implemented a bootloader according to the SPNA241 I've used link to examples from the document:
URL: git.ti.com/.../Bootloaders.
So I have an issue with TMDX570LC43HDK implementing code from the link.
Regards,
Sergey
Hi Sergey,
I didn't see this kind of issue when I tested the bootload on HDK before. I will do a test on LC43HDK.
Hi, I have a very similar problem.
After software reset, a read of SCI register (GCR1 of SCI1) causes Data Abort exception.
Please help, this is blocking for me.
Regards.
Hello,
The processor takes the data abort if data should be read from or written to a protected or faulty memory location. This could be because of:
Can you please check the data fault status (DFSR) register and address register in CP15 registers?
Hi Wang,
I’ve checked registers for the test code written in my first post. So following instruction gives an exception
00002c58: E5900004 ldr r0, [r0, #4]
Here is DFSR register:
CP15_DATA_FAULT_STATUS 0x00001008 DFSR [Core]
Rsv1 0000000000000000000 Reserved SBZ
SD 1 External Abort Only: AXI Decode(0) or AXI Slave (1)
RW 0 Read(0) or Write(1) Caused Abort
S 0 Status[4]
Rsv2 00 Reserved SBZ
DOMAIN 0000 Domain SBZ
STATUS 1000 Status[3:0] - 0x01=Algn, 0x00=BG, 0x0D=Perm, 0x08=SExt, 0x16=ASExt, 0x19=SECC, 0x18=ASECC, 0x02=DBG
Fault data register:
CP15_DATA_FAULT_ADDRESS 0xFFF7B850 DFAR [Core]
According to Cortex-R5 Technical Reference Manual DFSR register determines synchronous external abort:
0xFFF7B850 is address of HETDIN register
When I run the code on TMDS570LS31HDK ldr instruction uses the same address 0xFFF7B850 but exception doesn’t occur.
Regards,
Sergey
Hello Sergey,
Has the data abort issue been solved? What changes did you make to the original example code? I did another try on my bench, and it works without any issue.
Hello, Wang!
Thank you for your another trying on the bench.
I didn’t make any changes to the original bootloader example code for both TMDS570LS31HDK and TMDX570LC43HDK. I’ve got success for TMDS570LS31HDK and mentioned issue for TMDX570LC43HDK. I tried on two items of TMDX570LC43HDK.
So the same example code works on your bench successfully and has an issue on the purchased TMDX570LC43HDK. It allows to suppose some difference either in tested controllers or in IDE. I’ve used CCS Version: 10.0.0.00010, HALCoGen 04.07.01.
Did you use the same?
Just now I have no any idea how to solve the issue for TMDX570LC43HDK. I am testing the controllers to verify whether they can be used in projects of our company. The fact that required functions work on some bench will not be impressive evidence for our company management. I have to demonstrate key features for our projects on purchased development kits.
So if you know some idea how to solve the issue exactly for TMDX570LC43HDK let me know.
Regards, Sergey
Hello Sergey,
In your test, the application image has been uploaded and programmed to flash through the CAN bootloader. After the bootloader issues a SW reset, when the code jumps to the application?
In the bootloader example, the bootloader code checks if the GIOA[7] is pulled low, and if the application has been programmed successfully. If GIOA[7] is LOW or application has been programmed, the code will jump to application. Otherwise, it will call the update function for uploading data.
Hello, Wang!
In my case after SW reset the code really jumps to the application. And data abort exception occurs exactly in the application. So it’s possible to separate the data abort exception issue from the bootloader and consider sequence: SW reset - application.
Such example and explanation of it behavior I submitted in my first post dated Jun 19, 2020. On your request on DFSR register me and Lukasz Matecki answered in posts dated Jul 2, 2020 and Jul 7 2020. Registers analysis showed that after SW reset at least several memory areas of TMDX570LC4357 become protected. But on TMDS570LS31HDK the issue does not occur.
If you please, explain why does so simple test code work on TMDS570LS31HDK and does not work on TMDX570LC4357? Is it possible to solve the issue for TMDX570LC4357?
Regards, Sergey
Hello Sergey,
The bootloader works ok: download the image from PC, then program it to flash. The data abort may be caused by your application.
Did you test you code? The VECTORS in linker cmd file of the application should not be at 0x00000000. It should at the start address of your application.
VECTORS (X) : origin=0x00000000 length=0x00000020
Otherwise, it won't work.
In bootloader side, the interrupt should be disabled before calling the jumping instruction.
Another thing, is the ECC of application programmed? The Fapi_AutoEccGneration should be used when programming the application with the flash API. This flash API is called in Fapi_BlockProgram(0 function in bl_flash.c:
Fapi_issueProgrammingCommand((uint32_t *)dst,
(uint8_t *)src,
(uint32_t) bytes,
0,
0,
Fapi_AutoEccGeneration);
Hi Wang,
In my case, there is no flashing (I'm not using bootloader) but still I'm having a very similar problem.
Can this have something to do with ECC calculated by CCS / Uniflash?
Hello, Wang!
Here is code from my first post:
int main(void) { /* USER CODE BEGIN (3) */ int i, j; //Configure as output hetREG1->DIR = (1 << 5); while(1) { //three blinks before reset for(j = 0; j < 6; j++) { gioToggleBit(hetPORT1, 5); for(i = 0; i<5000000; i++); } //software reset systemREG1->SYSECR = (0x10) << 14; }; /* USER CODE END */ return 0; }
It works on TMDS570LS31HDK and does not work on TMDX570LC43HDK.
Can you check the code on your TMDX570LC43HDK , if you please? And if it will work, send the project for trying on my TMDX570LC43HDK.
Thank you in advance.
Regards,
Sergey
Hello Sergey,
I found the root cause. Actually it was caused by the code generated through HALCoGen. The SW Reset is not handled correctly in getResetSource(void) function and in sys_startup.c
1. Add SW Reset to getResetSource(void) :
else if ((SYS_EXCEPTION & (uint32)SW_RESET) !=0U)
{
rst_source = SW_RESET;
SYS_EXCEPTION = (uint32)SW_RESET;
}
2. Move SW_RESET to line 132
/*SAFETYMCUSW 62 S MR:15.2, 15.5 <APPROVED> "Need to continue to handle POWERON Reset" */
case DEBUG_RESET:
case EXT_RESET:
/* USER CODE BEGIN (6) */
case SW_RESET:
Attached is my CCS project:
Hello, Wang!
This resolved the issue.
It was important thing for our projects. I am very grateful and I want to thank you!
Regards, Sergey
Hi Wang.
This patch resolves my issue as well.
Please make sure the HalcoGen team is aware of this problem.
Many thanks,
Regards
Łukasz