Part Number: TMS570LS3137
Hi experts,
My customer erased the Bank0 region (0xE0000 to 128KB) using the F021API and
got a prefetch abort after calling the Fapi_isueAsyncCommandWithAddress() function.
CP15_INSTRUCTION_FAULT_STATUS was set to 0x409, so Synchronous Parity/ECC Error.
And CP15_INSTRUCTION_FAULT_ADDRESS is set to 0xC This is a vector region.
What is the cause of this error during Erase in Flash? I will check if there is any other information needed.
- F021 Flash API version :V2.01.01
- F021_API_CortexR4_BE_V3D16.lib
Best regards,
Sasaki