Part Number: TM4C1290NCPDT
Hi,
I'm configuring the DMA for writing from internal RAM to EPI. While this transfers works one time, I fail to clear the interrupt, so that it is constantly re-triggered. I thought EPIIntErrorClear(EPI0_BASE,EPI_INT_ERR_DMAWRIC)
should do the job, but does not. To be clear: I checked, if any other Interrupt occurs, but it is only the EPI_INT_DMA_TX_DONE one.
Any Help is welcome,
regards
Micky
My Code is
uint16_t auData[512]={1,2,3};
uint16_t* pDst =(uint16_t*)0x80000400;
ROM_uDMAChannelAttributeDisable(UDMA_CH21_EPI0TX, UDMA_ATTR_USEBURST);
ROM_uDMAChannelAttributeEnable(UDMA_CH21_EPI0TX, UDMA_ATTR_USEBURST);
ROM_uDMAChannelControlSet(UDMA_CH21_EPI0TX| UDMA_PRI_SELECT,
UDMA_SIZE_16| UDMA_SRC_INC_16 |
UDMA_DST_INC_NONE| UDMA_ARB_8);
ROM_uDMAChannelTransferSet(UDMA_CH21_EPI0TX | UDMA_PRI_SELECT,
UDMA_MODE_AUTO, auData,&pDst,
256);
ROM_uDMAChannelAssign(UDMA_CH21_EPI0TX);
ROM_uDMAIntClear(UDMA_CH21_EPI0TX);
ROM_uDMAChannelEnable(UDMA_CH21_EPI0TX);
ROM_uDMAChannelRequest(UDMA_CH21_EPI0TX);
EPIDMATxCount(EPI0_BASE,256);
And the Interrupt service handler
void vfnEpi0Handler()
{
uint32_t uStatus;
static uint32_t suEpiReady=0;
uint32_t uInts = ROM_EPIIntStatus(EPI0_BASE,true);
switch (uInts)
{
case EPI_INT_TXREQ:
suEpiReady++;
break;
case EPI_INT_RXREQ:
suEpiReady++;
break;
case EPI_INT_ERR:
suEpiReady++;
break;
case EPI_INT_DMA_TX_DONE:
suEpiReady++;
EPIIntErrorClear(EPI0_BASE,EPI_INT_ERR_DMAWRIC);
break;
case EPI_INT_DMA_RX_DONE:
suEpiReady++;
break;
default:
break;
}
uStatus = ROM_uDMAChannelModeGet(UDMA_CH21_EPI0TX);
if(uStatus == UDMA_MODE_STOP)
{
// DMA Ready
suEpiReady++;
}
};